Skip to main content
Associate III
December 4, 2023
Question

STM32F4 Discovery dual adc timer triggered

  • December 4, 2023
  • 5 replies
  • 1990 views

Good evening everyone, I'm trying to sample two signals through TIM2 using ADC in dual regular simultaneous mode with a trigger from TIM2. When configuring the ADC in dual mode, it only reads and performs a single conversion on one channel. Does anyone have any idea what I might be doing wrong?

 

//Start of Multimode
HAL_ADC_Start(&hadc2);
 if(HAL_ADCEx_MultiModeStart_DMA(&hadc1 , (uint32_t *)dmaBuffer, 100) != HAL_OK){
 	 Error_Handler();
 }
if(HAL_TIM_Base_Start(&htim2) != HAL_OK){
	 Error_Handler();
 }


// Timer 2 Config
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 1;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */

}

// ADC1 
hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

//ADC2
hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.ScanConvMode = DISABLE;
 hadc2.Init.ContinuousConvMode = DISABLE;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
December 4, 2023

Period of 1 seems a bit wishful

Don't think it needs master/slave mode enable

Suspect you need to configure multi-mode

Did this successfully on the F4, but was using the SPL

 

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
davidecAuthor
Associate III
December 4, 2023

Multi-mode is enabled :

static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ENABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_REGSIMULT;
 multimode.DMAAccessMode = ADC_DMAACCESSMODE_2;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.ScanConvMode = ENABLE;
 hadc2.Init.ContinuousConvMode = ENABLE;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DMAContinuousRequests = ENABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

The thing I don't understand is why it only reads one channel and then with the period at 1 it works fine.

TDK
December 4, 2023

Perhaps show the full code. Why do you think it only performs one of the conversions?

"If you feel a post has answered your question, please click ""Accept as Solution""."
davidecAuthor
Associate III
December 4, 2023

Because i'm printing the signals that i'm acquiring

davidecAuthor
Associate III
December 4, 2023
/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "string.h"
#include "stdio.h"
#include "stdlib.h"
#include "stm32f4xx_hal.h"
#include "AD9833.h"

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc2;
DMA_HandleTypeDef hdma_adc1;
DMA_HandleTypeDef hdma_adc2;

TIM_HandleTypeDef htim2;

UART_HandleTypeDef huart2;
DMA_HandleTypeDef hdma_usart2_tx;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_ADC2_Init(void);
static void MX_TIM2_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint32_t dmaBuffer[100];
uint32_t i;
uint16_t buf1[100];
uint16_t buf2[100];
uint32_t count;

uint8_t flag = 1;
uint8_t flag_c = 0;
char str[16];
char space[16] = "*\r\n";
uint32_t u=0;
uint32_t c1=0;
uint32_t c2 = 0;





/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_USART2_UART_Init();
 MX_ADC2_Init();
 MX_TIM2_Init();
 /* USER CODE BEGIN 2 */


 HAL_ADC_Start(&hadc2);
 if(HAL_ADCEx_MultiModeStart_DMA(&hadc1 , (uint32_t *)dmaBuffer, 100) != HAL_OK){
 	 Error_Handler();
 }


 
 if(HAL_TIM_Base_Start(&htim2) != HAL_OK){
	 Error_Handler();
 }

 
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {

 	 if (flag == 1){
 		 
 		 
 		 for (i = 0; i <100; i++) {
 			 buf1[i] = (uint16_t)(dmaBuffer[i] & 0x0000FFFF);
 		 buf2[i] = (uint16_t)(dmaBuffer[i] >> 16);
 		}

 		 for(c1=0;c1<100;c1++){
 			 sprintf(str, "%u \r\n",((uint16_t*)buf1)[c1]); // conversion in str of value
 		 HAL_UART_Transmit(&huart2, (uint8_t*)str, strlen(str), HAL_MAX_DELAY);

 HAL_Delay(5);

 }
 HAL_UART_Transmit(&huart2,(uint8_t *)space,strlen(space),10);


 for(c2=0;c2<100;c2++){
 	 sprintf(str, "%u \r\n",((uint16_t*)buf2)[c2]); // conversion in str of value
 HAL_UART_Transmit(&huart2, (uint8_t*)str, strlen(str), HAL_MAX_DELAY);

 HAL_Delay(5);

 }
 HAL_UART_Transmit(&huart2,(uint8_t *)space,strlen(space),10);
 //count++;
 		 flag = 0;
 	 }
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 72;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV4;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ENABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_REGSIMULT;
 multimode.DMAAccessMode = ADC_DMAACCESSMODE_2;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.ScanConvMode = ENABLE;
 hadc2.Init.ContinuousConvMode = ENABLE;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DMAContinuousRequests = ENABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 1;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream6_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream6_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);
 /* DMA2_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
 /* DMA2_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);

 /*Configure GPIO pins : PA5 PA6 PA7 */
 GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PB6 */
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */



void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
	
	flag = 1;
	

	HAL_ADC_Start(&hadc2);
	if(HAL_ADCEx_MultiModeStart_DMA(&hadc1 , (uint32_t *)dmaBuffer, 100) != HAL_OK){
		Error_Handler();
	 }




 


}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */