cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F767ZI Arduino subset has wrong spacing

BSchm.0
Associate II

I tried to plug a shield arduino RS485 shield that fits on NUCLO-F401RE without any chance because of wrong spacing :thumbs_down:

2 REPLIES 2
MNapi
Senior III

those pins are spaced I believe 2.5 mm which is standard for the connectors. Use jumper connectors. for example the arduino mcufriend tft display plugs in without problem. which is very nice combo. Except the fact I couldn't not find any libraries to light it up.

Uwe Bonnes
Principal III

Are you sure you tried to plug it in the right connectors with the right orientation? We already used arduino shield on the NUCLEO-F767ZI with no problem.