cancel
Showing results for 
Search instead for 
Did you mean: 

Someone have info, project or something to help about EPD display's. I hate the use of ARDUINO IDE, I'm an old man that want to understand the code, I don't like the ARDUINO "magic", because it use a lot of space and is very difficult to optimize

PGinh.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

There's some stuff out there on "stm32 epd". Here's one:

https://github.com/soonuse/epd-library-stm32

If you feel a post has answered your question, please click "Accept as Solution".

Thanks. It does not have the size that I need 3.7

Anyway, I'm going to start with this.

Going to need be more specific about the make, model, part of the screen and the controller ICs involved.

If you can get those, you can perhaps unpack what the Arduino libraries are doing, and what portions are need to initialize the display, and transfer frames.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes, thank you. I bought a NUCLEOF411 (maybe too big for this) and the EXT3 module with EPAPER 3,7" for PermasiveDisplay.

I need to Test, set Up and include some code.

I develop with Microchip uC since 18 years (started with assembler). This is my first time with STM

This?

https://www.tme.eu/Document/d3f49245a0afc5ca823e68cceafbb59f/WSH-18057.pdf

If using I2C, dig up some STM32 I2C examples

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..