2024-04-09 02:33 PM - last edited on 2024-04-09 02:51 PM by mƎALLEm
I am using CAN1 pins to Connect to the driver board (SN65HVD230).
All Voltages are good.
I am using 2 PCAN dongles with 120 Ohm terminations at both ends of the BUS with the Nucleo CAN shown above in the middle of the bus.
I ported the code from the following project;
>TX Mailbox used: 0x1
t
>TX Mailbox used: 0x2
s
>MCR: 0x30
Can State: 0x2
Interrupts: 0x1007F, msr flags: 0xC00 , tsr flags: 0x52000000, rf0r flags: 0x0, rf1r flags: 0x0, esr flags: 0x0
The Tx message is not getting out.
Also I have a PCAN message being transmitted on one PCAN dongle and the other PCAN Dongle is receiving the message fine.
The Nucleo pcb does not see the message at all.
I am using the default clock setup for the NUCLEO board
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 384;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 8;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
The CAN setup for 250 K
/**
* @brief CAN1 Initialization Function
* None
* @retval None
*/
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
HAL_StatusTypeDef HAL_error;
CAN_FilterTypeDef sFilterConfigCAN1;
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 12;
hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = ENABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
sFilterConfigCAN1.FilterBank = 0;
sFilterConfigCAN1.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfigCAN1.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfigCAN1.FilterIdHigh = 0x0000;
sFilterConfigCAN1.FilterIdLow = 0x0000;
sFilterConfigCAN1.FilterMaskIdHigh = 0x0000;
sFilterConfigCAN1.FilterMaskIdLow = 0x0000;
sFilterConfigCAN1.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfigCAN1.FilterActivation = ENABLE;
sFilterConfigCAN1.SlaveStartFilterBank = 14;
HAL_error = HAL_CAN_ConfigFilter(&hcan1, &sFilterConfigCAN1);
if (HAL_error != HAL_OK)
{
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
HAL_error = HAL_CAN_Start(&hcan1);
if (HAL_error != HAL_OK)
{
Error_Handler();
}
/*##-4- Activate CAN RX notification #######################################*/
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_FULL);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_FULL);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_OVERRUN);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_TX_MAILBOX_EMPTY);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_OVERRUN);
HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_WAKEUP);
if (HAL_error != HAL_OK)
{
Error_Handler();
}
/* USER CODE END CAN1_Init 2 */
}
Solved! Go to Solution.
2024-04-09 02:48 PM - edited 2024-04-09 03:01 PM
Hello,
1- Silent mode?
hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;
2- You need to check your GPIOs: are you sure about the correct GPIOs connected to the transceiver (correct alternate functions)?
3- Are you sure about your bitrate?
4- You need to validate your tranceiver module:
Are you seeing frames on CAN_TX and CAN_RX? If not, you have an issue with your module. Are you sure the transceiver is power supplied? check the voltage on its pins.
PS: in next time please use </> button to insert your code.
Thanks.
2024-04-09 02:48 PM - edited 2024-04-09 03:01 PM
Hello,
1- Silent mode?
hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;
2- You need to check your GPIOs: are you sure about the correct GPIOs connected to the transceiver (correct alternate functions)?
3- Are you sure about your bitrate?
4- You need to validate your tranceiver module:
Are you seeing frames on CAN_TX and CAN_RX? If not, you have an issue with your module. Are you sure the transceiver is power supplied? check the voltage on its pins.
PS: in next time please use </> button to insert your code.
Thanks.
2024-04-09 07:29 PM
How do you know if one of the Activate CAN RX notification section returns HAL_ERROR but gets set to HAL_OK towards the end?
Did you enable the NVIC? What is the APB1 clock frequency?
2024-04-10 12:09 PM
I changed to different transceiver and fixed the Port Pin selection on the CAN_TX and CAN_RX. I had Pin 0 and Pin 1 configured to the alternate selection but it was on port G instead of port D. I also had the CAN_H and CAN_L swapped. I am now working great. Thanks SoftLit and Karl for your help.