cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F412ZG CAN Communication, No RX and No tx

JDOG
Associate III

I am using CAN1 pins to Connect to the driver board (SN65HVD230).

 

JDOG_3-1712698313675.png

 

0405241626~2.jpg

 All Voltages are good.

I am using 2 PCAN dongles with 120 Ohm terminations at both ends of the BUS with the Nucleo CAN shown above in the middle of the bus. 

I ported the code from the following project;

JDOG_0-1712696721291.png

 


>TX Mailbox used: 0x1
t
>TX Mailbox used: 0x2
s
>MCR: 0x30
Can State: 0x2
Interrupts: 0x1007F, msr flags: 0xC00 , tsr flags: 0x52000000, rf0r flags: 0x0, rf1r flags: 0x0, esr flags: 0x0

The Tx message is not getting out.

 

Also I have a PCAN message being transmitted on one PCAN dongle and the other PCAN Dongle is receiving the message fine.

JDOG_1-1712698012460.pngJDOG_2-1712698114551.png

 

 

The Nucleo pcb does not see the message at all.

I am using the default clock setup for the NUCLEO board

 

 

 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 8;

RCC_OscInitStruct.PLL.PLLN = 384;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;

RCC_OscInitStruct.PLL.PLLQ = 8;

RCC_OscInitStruct.PLL.PLLR = 2;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)

{

Error_Handler();

}

}

 

The CAN setup for 250 K

/**

* @brief CAN1 Initialization Function

*  None

* @retval None

*/

static void MX_CAN1_Init(void)

{

 

/* USER CODE BEGIN CAN1_Init 0 */

HAL_StatusTypeDef HAL_error;

CAN_FilterTypeDef sFilterConfigCAN1;

 

/* USER CODE END CAN1_Init 0 */

 

/* USER CODE BEGIN CAN1_Init 1 */

 

/* USER CODE END CAN1_Init 1 */

hcan1.Instance = CAN1;

hcan1.Init.Prescaler = 12;

hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;

hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;

hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;

hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;

hcan1.Init.TimeTriggeredMode = DISABLE;

hcan1.Init.AutoBusOff = DISABLE;

hcan1.Init.AutoWakeUp = ENABLE;

hcan1.Init.AutoRetransmission = DISABLE;

hcan1.Init.ReceiveFifoLocked = DISABLE;

hcan1.Init.TransmitFifoPriority = DISABLE;

if (HAL_CAN_Init(&hcan1) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN CAN1_Init 2 */

 

sFilterConfigCAN1.FilterBank = 0;

sFilterConfigCAN1.FilterMode = CAN_FILTERMODE_IDMASK;

sFilterConfigCAN1.FilterScale = CAN_FILTERSCALE_32BIT;

sFilterConfigCAN1.FilterIdHigh = 0x0000;

sFilterConfigCAN1.FilterIdLow = 0x0000;

sFilterConfigCAN1.FilterMaskIdHigh = 0x0000;

sFilterConfigCAN1.FilterMaskIdLow = 0x0000;

sFilterConfigCAN1.FilterFIFOAssignment = CAN_RX_FIFO0;

sFilterConfigCAN1.FilterActivation = ENABLE;

sFilterConfigCAN1.SlaveStartFilterBank = 14;

 

HAL_error = HAL_CAN_ConfigFilter(&hcan1, &sFilterConfigCAN1);

 

if (HAL_error != HAL_OK)

{

Error_Handler();

}

 

 

 

/*##-3- Start the CAN peripheral ###########################################*/

HAL_error = HAL_CAN_Start(&hcan1);

 

if (HAL_error != HAL_OK)

{

Error_Handler();

}

 

/*##-4- Activate CAN RX notification #######################################*/

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_FULL);

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING);

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_FULL);

 

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_OVERRUN);

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_TX_MAILBOX_EMPTY);

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_OVERRUN);

 

 

HAL_error = HAL_CAN_ActivateNotification(&hcan1, CAN_IT_WAKEUP);

 

 

if (HAL_error != HAL_OK)

{

Error_Handler();

}

/* USER CODE END CAN1_Init 2 */

 

}

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

1- Silent mode?

 

hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;

 

2- You need to check your GPIOs: are you sure about the correct GPIOs connected to the transceiver (correct alternate functions)?

3- Are you sure about your bitrate?

4- You need to validate your tranceiver module:

Are you seeing frames on CAN_TX and CAN_RX? If not, you have an issue with your module. Are you sure the transceiver is power supplied? check the voltage on its pins.

PS: in next time please use </> button to insert your code.

Thanks.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

3 REPLIES 3
SofLit
ST Employee

Hello,

1- Silent mode?

 

hcan1.Init.Mode = CAN_MODE_SILENT; //CAN_MODE_NORMAL;

 

2- You need to check your GPIOs: are you sure about the correct GPIOs connected to the transceiver (correct alternate functions)?

3- Are you sure about your bitrate?

4- You need to validate your tranceiver module:

Are you seeing frames on CAN_TX and CAN_RX? If not, you have an issue with your module. Are you sure the transceiver is power supplied? check the voltage on its pins.

PS: in next time please use </> button to insert your code.

Thanks.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Karl Yamashita
Lead III

How do you know if one of the Activate CAN RX notification section returns HAL_ERROR but gets set to HAL_OK towards the end?

Did you enable the NVIC? What is the APB1 clock frequency?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
JDOG
Associate III

0410241400~2.jpg

 I changed to different transceiver and fixed the Port Pin selection on the CAN_TX and CAN_RX. I had Pin 0 and Pin 1 configured to the alternate selection but it was on port G instead of port D. I also had the CAN_H and CAN_L swapped. I am now working great. Thanks SoftLit and Karl for your help.