2018-03-15 11:40 PM
Hi Forum. I am new to the H7 line of processors and the first thing I tried is getting printf() output on the traceswo pin of my nucleo-H743ZI. What I have tried:
1. The 'Everything out of the box' way:
Use cubeMX to configure sys to async trace, configure clocks, enable master clock out (to verify clock speed with a logic analyser).
Import the project to atollic truestudio and configure debugging to use the SWV, with the specific baudrate and core clock.
Write simples mainloop:
while(1) {
ITM_Sendchar('T');
delay(xxx);
}
Start a debugging session, configure trace port 0 and start tracing -> no output in atollic truestudio, no output on PB3 (verified with logic analyser)
2. The 'Do some manual work and hope the rest will resolve' way:
Same as above, with the exception of enabling the ITM unit manually:
CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk;
CoreDebug->DEMCR |= CoreDebug_DEMCR_VC_CORERESET_Msk;
ITM->LAR = 0xC5ACCE55; // Unlock Lock Access Registers
ITM->TCR |= ITM_TCR_DWTENA_Msk;ITM->TCR |= ITM_TCR_SYNCENA_Msk;ITM->TER |= 0x01; // Port 0ITM->TCR |= ITM_TCR_ITMENA_Msk;
Start debug session, enable tracing in atollic studio, THEN call my own init function - since the debugger overwrites the register values -> No traceswo output
3. The 'Do another variation of the non-working example' way:
Same as above, but I let the debugger handle the initialization and have the processor my init code before tracing is enabled through atollic stuido
-> Same result
4. The 'Try to do it by the book' way:
Here I really failed. What I tried:
Configure ITM manually, configure the SWO and SWTF unit manually.
Here my problem is that I do not know where SWO and SWTF are found in memory. The reference manual tells me that I can look up these adresses through the System ROM tables at adress 0xE00E0000.
However acessing these yields a fault -- Have not implemented the different faults, so i can not tell which is the one thats biting my ***! So I thought: Maybe I need to access these in priviledged mode.. same error.
(Atollic truestudio version - if that matters):
Atollic TrueSTUDIO� for STM32, Built on Eclipse Neon.1a.
Version: 9.0.0
Build id: 20180117-1023
Has someone a working example for trace output on the traceswo line on the nucleo-h743zi using atollic truestudio?
Any help or suggestions are apprechiated!
Florian
Addendum:
I received a response from Atollic.
XXXXX XXXXXXX
(Atollic Support)
Mar 16, 09:17 CET
Dear Florian,
There is a known problem with the STM32H7 which we have a ticket for at the moment. We hope to have this fixed until the next release. However, we haven't had a response from the correct ST department just yet if there's a problem with the MCU itself or if we've made a faulty configuration in the software somewhere. We're going to try to reach out again for a response.Best regards
XXXXXX, Atollic Support Team#atollic-truestudio #itm-swo-trace #nucleo-h743zi
2018-05-18 4:27 PM
Like this?
2018-05-21 6:50 AM
Exactly.
2018-05-21 7:25 AM
Ok, that didn't seem viable of the STM32H743I-EVAL, didn't see any solder-bridge/jumpers there, will try on NUCLEO-H743ZI later.
2018-06-18 11:25 PM
Short Bump + a short reminder, that theese issues are not solved.
Looking at you ST. It has been over three months now. The errata sheet from May,2018 does not include a note, or any advisory and the datasheet has not updated since November,2017.
That's very discouraging. Is someone working on it?
2018-06-19 1:31 AM
Well a mob is starting to assemble
https://community.st.com/0D50X00009XkhURSAZ
2018-06-21 9:38 AM
https://community.st.com/0D50X00009nNBBHSA4
2018-08-09 4:06 AM
Anyone managed to get link above working (or below if you are upside down)?
2018-08-09 4:46 AM
It didn't survive the jump to the new forum, currently still exists here
https://st-microelectronics.jiveon.com/docs/DOC-2098-how-to-use-the-swo-on-stm32h7-devices
I condensed it down to this
void SWD_Init(void)
{
*(__IO uint32_t*)(0x5C001004) |= 0x00700000; // DBGMCU_CR D3DBGCKEN D1DBGCKEN TRACECLKEN
//UNLOCK FUNNEL
*(__IO uint32_t*)(0x5C004FB0) = 0xC5ACCE55; // SWTF_LAR
*(__IO uint32_t*)(0x5C003FB0) = 0xC5ACCE55; // SWO_LAR
//SWO current output divisor register
//This divisor value (0x000000C7) corresponds to 400Mhz
//To change it, you can use the following rule
// value = (CPU Freq/sw speed )-1
*(__IO uint32_t*)(0x5C003010) = ((SystemCoreClock / 2000000) - 1); // SWO_CODR
//SWO selected pin protocol register
*(__IO uint32_t*)(0x5C0030F0) = 0x00000002; // SWO_SPPR
//Enable ITM input of SWO trace funnel
*(__IO uint32_t*)(0x5C004000) |= 0x00000001; // SWFT_CTRL
//RCC_AHB4ENR enable GPIOB clock
*(__IO uint32_t*)(0x580244E0) |= 0x00000002;
// Configure GPIOB pin 3 as AF
*(__IO uint32_t*)(0x58020400) = (*(__IO uint32_t*)(0x58020400) & 0xffffff3f) | 0x00000080;
// Configure GPIOB pin 3 Speed
*(__IO uint32_t*)(0x58020408) |= 0x00000080;
// Force AF0 for GPIOB pin 3
*(__IO uint32_t*)(0x58020420) &= 0xFFFF0FFF;
}
2019-02-04 11:39 AM
We might have to revisit this on the ST-LINK V3SET and Keil, the V3 is using a 15 MHz SWV clock, not 2 MHz, so the math changes. This was on a 120 MHz L4+ board, so the frequency/multiples might be different in other environments or use cases.