cancel
Showing results for 
Search instead for 
Did you mean: 

NMI Fault While Debugging (STM32G474 nucleo board)

toofer25
Associate

Hello,

I keep getting an NMI fault when I attempt to read a variable with gdb (either with a mouseover on a variable in STM32CubeIDE or the print [var] command in gdb). I'm not seeing anything useful when I view the microprocessor registers after the fault.

I'm using the stm32g474 hal library along with a linker, startup file, and interrupt _it files that are normally generated by default with the STM32CubeMX software for a G474 nucleo board. However, I'm using cmake 2.47.6 and the arm gcc/g++ toolchain 11.2-2022.02 for the build process.

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

According the the user manual, there are three sources to generate an NMI:

  1. Clock security system (CSS)
  2. Flash ECC error
  3. Parity check SRAM1/CCM SRAMs. 

I suspect the 3rd choice: Parity check

So check the user option byte SRAM_PE value in option bytes menu in STM32CubeProgrammer.



To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello,

According the the user manual, there are three sources to generate an NMI:

  1. Clock security system (CSS)
  2. Flash ECC error
  3. Parity check SRAM1/CCM SRAMs. 

I suspect the 3rd choice: Parity check

So check the user option byte SRAM_PE value in option bytes menu in STM32CubeProgrammer.



To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.