cancel
Showing results for 
Search instead for 
Did you mean: 

Newly-installed Atollic TrueStudio gives eclipse-related errors

Dkenn.1
Associate

I just installed Atollic TrueStudio on a new PC. I am getting eclipse-related errors when I try to run the program. I have attached the log.

The first few lines of the log are below. full error log is attached

 

!SESSION 2022-04-06 15:16:19.728 -----------------------------------------------

eclipse.buildId=unknown

java.version=1.8.0_181

java.vendor=Oracle Corporation

BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US

Command-line arguments: -os win32 -ws win32 -arch x86

 

!ENTRY com.atollic.truestudio.productmanager 1 0 2022-04-06 15:16:20.978

!MESSAGE Loading product manager

 

!ENTRY com.atollic.truestudio.productmanager 1 0 2022-04-06 15:16:20.982

!MESSAGE OS info: Windows 10, 10.0, x86

 

!ENTRY org.eclipse.osgi 4 0 2022-04-06 15:16:21.056

!MESSAGE An error occurred while automatically activating bundle org.eclipse.core.resources (176).

!STACK 0

org.osgi.framework.BundleException: Exception in org.eclipse.core.resources.ResourcesPlugin.start() of bundle org.eclipse.core.resources.

at org.eclipse.osgi.internal.framework.BundleContextImpl.startActivator(BundleContextImpl.java:795)

at org.eclipse.osgi.internal.framework.BundleContextImpl.start(BundleContextImpl.java:724)

at org.eclipse.osgi.internal.framework.EquinoxBundle.startWorker0(EquinoxBundle.java:932)

at org.eclipse.osgi.internal.framework.EquinoxBundle$EquinoxModule.startWorker(EquinoxBundle.java:309)

at org.eclipse.osgi.container.Module.doStart(Module.java:581)

at org.eclipse.osgi.container.Module.start(Module.java:449)

1 ACCEPTED SOLUTION

Accepted Solutions
raptorhal2
Lead

The installation resources guide says 64 bit windows required for installation on W8 and W10. The log shows W32.

Cheers, Hal

View solution in original post

1 REPLY 1
raptorhal2
Lead

The installation resources guide says 64 bit windows required for installation on W8 and W10. The log shows W32.

Cheers, Hal