2022-04-06 8:29 AM
2022-04-06 8:36 AM
SPI -> DMA -> SRAM -> ?
That way you will only get DMA (half-) complete interrupts, how often depends on your buffer size.
Depending on what you want to do with the ADC data, I'd recommend an STM32 with DMA supporting double buffering.
2022-04-06 8:56 AM
Hi, yes that is my intention. But my isues is i need to use the chip select for an input to the adc as a conversion start trigger. But when configureing the spi as a master format motorola and enable the NSS i need to enable and disable the spi to get NSS toggling.
/* Disable all peripherals for now*/
DMA2_Stream5->CR = 0;
DMA2_Stream2->CR = 0;
TIM1->CR1 = 0;
SPI1->CR1 = 0;
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
/* DMA2 SPI1 receive */
/* Setting source & target pointer for rx */
LL_DMA_SetMemoryAddress(DMA2, LL_DMA_STREAM_2, (uint32_t)adc_data);
LL_DMA_SetPeriphAddress(DMA2, LL_DMA_STREAM_2, (uint32_t)&SPI1->DR);
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_2, ADC_VALUE_COUNTS);
DMA2_Stream2->FCR = 0;
/* enable spi to do req on dma */
LL_SPI_EnableDMAReq_RX(SPI1);
/* DMA2 start now for rx*/
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_2);
/* start SPI now */
LL_SPI_Enable(SPI1);
/* Setting source & target pointer for tx */
LL_DMA_SetMemoryAddress(DMA2, LL_DMA_STREAM_5, (uint32_t)adc_channel);
LL_DMA_SetPeriphAddress(DMA2, LL_DMA_STREAM_5, (uint32_t)&SPI1->DR);
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_5, ADC_CHANNEL_COUNTS);
DMA2_Stream5->FCR = 0;
temp = DMA2_Stream5->CR;
/* DMA2 start now for tx*/
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_5);
/* start TIM1 now and start update event*/
LL_TIM_EnableDMAReq_UPDATE(TIM1);
LL_TIM_EnableCounter(TIM1);well this runs in an endless loop but with no control of the chip select. How could i have control of the NSS pin without using interrupts, because other wise i could do all in the interrupt.
Greetings
2022-04-06 9:16 AM
Then it's probably not going to work ideally.
For these types of things people typically add glue logic, in the form of a state-machine, or other combinatorial logic, in a CPLD, or something, to smooth the disparity in expectations, and can do so at wire rates.
2022-04-06 2:10 PM
Which STM32?
> How could i have control of the NSS pin without using interrupts
Using timers.
One way to pull this off is to generate both the framing and SPI SCK from two master-slave-coupled timers, and feed it back externally to SPI set as slave.
Sometimes this sort of protocols can be pulled off quite easily using the SAI module.
JW