ā2022-08-22 2:36 AM
I am able to FIT 139KB .bin files , 11KB extra??
stm32f105RBt6 B should indicate128KB flash
What is going on... is it safe to use this extra memory?
How much extra memory does this chip have?
Solved! Go to Solution.
ā2022-08-22 3:05 AM
No, it is not safe to use. But you can also read e.g. this post where I described why.
Does it answer your question?
Regards
/Peter
ā2022-08-22 3:05 AM
No, it is not safe to use. But you can also read e.g. this post where I described why.
Does it answer your question?
Regards
/Peter
ā2022-08-22 3:07 AM
Thanks @Peter BENSCHā , i do have realiable sourced original STM32 parts.
i wonder why only some Flash is guaranteed to have full functionality
ā2022-08-22 3:53 AM
The untested flash area may well be fully functional, but the emphasis here is clearly on "may". In the production of the chips, it is quite possible that individual blocks of the untested area have errors or quality problems that do not affect the rest, but are not found due to the lack of testing. The function of the untested area is therefore not guaranteed and can deviate in several parameters: temperature capability, number of write cycles, etc.
In addition, the next batch can always contain a further cost-optimised die in which the untested area has been removed and thus the silicon area reduced to the minimum.
Clear now?
Regards
/Peter
ā2022-08-22 4:07 AM
crystal water clear, thanks @Peter BENSCHā
ā2022-08-22 4:10 AM
:smiling_face_with_smiling_eyes:
Cheers! uhm... Ā”Salud!