2019-09-16 07:34 AM
thanks for answering my previous question so according to this i supplied voltages from 0v to 5v and i got following step sizes(if i am correct) what i observed is it stops measuring after 2.5v so does it mean its measuring range is from 0-2.5v / can i connect vdd/vref pin externally to any voltage and can i measure to that extent without damaging the board can any one clarify this to me and thanks in advance and you can find the excel sheet below thanks once again
2019-09-17 05:30 AM
I have gone through the manuals of STM32F4 and understand that VREF+/VREF- determines the measurement range. I have STM32F4 Discovery board for which VREF+ (pin 21) is not exposed on pin headers and seems to be internally set to 2.5 v and is the reason for measurement range of ADC. I want to take full advantage of measurement range from 0 to 3.3V. So, believe VREF needs to be updated (probably to 3.3V?) Kindly help in understanding this measurement range/VREF adjustment (and also impact on other peripherals with modified VREF if I can modify....).