Skip to main content
Associate II
October 16, 2024
Solved

ultrasonic A02YYUW not working in STM32L443VCT6

  • October 16, 2024
  • 10 replies
  • 1973 views

Hi,

I try to comuunicate between STM32L443VCT6  and ultrasonic A02YYUW (By UART1) 

Just to make sure that the ultrasonic is working ok, i tested it by UART1 with model: stm32 neucler f441 and everthing works ok.

 

This is the code for the STM32L443VCT6:

 

 

 

#include "main.h"
#include "string.h"
#include "stdio.h"
#include "stdlib.h"
#include <stdbool.h>

UART_HandleTypeDef huart1;

uint8_t data[4] = {0}; // Buffer to hold the 4 bytes from the sensor
float distance = 0.0;

void SystemClock_Config(void);
void MX_GPIO_Init(void);
void MX_USART2_UART_Init(void);

int main(void) {
 HAL_Init();
 SystemClock_Config(); // Use internal oscillator (MSI)
 MX_GPIO_Init();
 USART1_UART_Init();




 /* Infinite loop */
 while (1) {
 /* Wait for the start corrector (0xFF) */
 do {
 HAL_UART_Receive(&huart1, &data[0], 1, HAL_MAX_DELAY);
 } while (data[0] != 0xFF);

 /* Clear the data array before receiving new data */
 //clearDataArray();

 /* Start receiving 3 more bytes of data */
 for (int i = 1; i < 4; i++) {
 HAL_UART_Receive(&huart1, &data[i], 1, HAL_MAX_DELAY); // Blocking receive
 }

 /* Process the sensor data */
 processSensorData();

 HAL_Delay(100); // Delay for sensor refresh (similar to Arduino delay)
 }

 /* Infinite loop */
 while (1) {
 // Keep running if needed, or you can add additional functionality
 }
}



void processSensorData(void) {
 /* Validate the checksum */
 int sum = (data[0] + data[1] + data[2]) & 0x00FF;
 // if (sum == data[3]) {
 /* Calculate the distance */
 distance = (data[1] << + data[2]; // Combine the two bytes into a 16-bit value
 distance = distance / 10.0; // Convert distance to cm

 /* Blink the LED to indicate valid data */

 if(distance<10){

 	HAL_Delay(500);
 }
 // } else {
 // Handle checksum error (optional)
 //}
}



/* GPIO Initialization Function */
 void MX_GPIO_Init(void) {
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* Enable GPIO clock for PA9 and PA10 (USART1 TX/RX pins) */
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* Configure PA9 (USART1 TX) */
 GPIO_InitStruct.Pin = GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; // Alternate function push-pull
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART1; // AF7 for USART1
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* Configure PA10 (USART1 RX) */
 GPIO_InitStruct.Pin = GPIO_PIN_10;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; // Alternate function push-pull
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART1; // AF7 for USART1
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}


 void USART1_UART_Init(void) {
 /* Enable USART1 clock */

 	 /* GPIO Ports Clock Enable */
 	 __HAL_RCC_GPIOC_CLK_ENABLE();
 	 __HAL_RCC_GPIOA_CLK_ENABLE();
 	 __HAL_RCC_GPIOB_CLK_ENABLE();
 	 __HAL_RCC_GPIOE_CLK_ENABLE(); // Enable clock for Port E
 	 __HAL_RCC_GPIOD_CLK_ENABLE();

 __HAL_RCC_USART1_CLK_ENABLE();

 /* Initialize USART1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 9600;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;

 if (HAL_UART_Init(&huart1) != HAL_OK) {
 Error_Handler(); // Handle initialization error
 }
 }


 /* System Clock Configuration */
 void SystemClock_Config(void) {
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 // Configure the main internal regulator output voltage
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) {
 Error_Handler();
 }

 // Initializes the RCC Oscillators according to the specified parameters
 // Here we use the internal Multi-Speed Internal (MSI) oscillator
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; // MSI range 6 corresponds to 4 MHz
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 40;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
 Error_Handler();
 }

 // Initializes the CPU, AHB, and APB buses clocks
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
 | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) {
 Error_Handler();
 }

 // Enable MSI Auto-calibration
 HAL_RCCEx_EnableMSIPLLMode();
 }



/* Error Handler */
void Error_Handler(void) {
 __disable_irq();
 while (1) {
 // Blink the LED to indicate an error

 HAL_Delay(500);
 }
}

 

 

This topic has been closed for replies.
Best answer by roystm321

Thank Everyone for you fast response,

I Solved it, i do not understand why..., but the "HAL_MAX_DELAY" blocked the receiveing data,

 

So i modify it to 300ms and now i get response from the ultrasonic, 

There is a tiny glitch, that seldom. the sensor not detect the correct value.

 

Is there any settings in the code i sent, that i need to pay attention?

 

Thanks!  

10 replies

Tesla DeLorean
Guru
October 16, 2024

Post not terribly enlightening..

How's this all wired up, show a schematic or wiring diagram.

Describe expected behaviour. Show salient portion of datasheet. Link to data sheet.

What do you actually observe?

Any data? The wrong data? Looked at signals with a scope or logic analyzer?

Any helpful observations you can share?

"Not Working" is an unhelpful diagnosis / symptom.  What's happening vs what's not..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
October 16, 2024

As @Tesla DeLorean said, your post is not very clear.

Are you saying that you have this working on an ST Neucleo-F441 board, but not on your own custom board, with an STM32L443VCT6?

If so, you'll need to

  1. Confirm that this is the "ultrasonic A02YYUW": 
    https://wiki.dfrobot.com/_A02YYUW_Waterproof_Ultrasonic_Sensor_SKU_SEN0311 
  2. Show how you had this connected-up on the Nucleo
  3. Post the schematic of your custom board - including how the "ultrasonic" is connected
  4. Describe what testing you have done on your custom board:
    1. Is the board working at all?
    2. Is the UART transmitting and/or receiving?
    3. etc, ...

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
roystm321AuthorBest answer
Associate II
October 16, 2024

Thank Everyone for you fast response,

I Solved it, i do not understand why..., but the "HAL_MAX_DELAY" blocked the receiveing data,

 

So i modify it to 300ms and now i get response from the ultrasonic, 

There is a tiny glitch, that seldom. the sensor not detect the correct value.

 

Is there any settings in the code i sent, that i need to pay attention?

 

Thanks!  

Andrew Neil
Super User
October 16, 2024

@roystm321 wrote:

the "HAL_MAX_DELAY" blocked the receiveing data,


Hmmm...,  I've seen that somewhere before but can't quite remember where or what the issue was.

I think the maximum actual wait is HAL_MAX_DELAY - 1

Anyhow, as it's solved your problem, please mark the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
roystm321Author
Associate II
October 16, 2024

It looks like that sometime not all the data in the array comes:

 HAL_UART_Receive(&huart1, &data[i], 1, HAL_MAX_DELAY); 

and then this prevent from the code continue to run..

roystm321Author
Associate II
October 16, 2024

Ok i will try it, thanks