2023-10-26 11:28 PM - edited 2023-10-26 11:30 PM
Hi, which is the maximum analog output voltage from the STM32H723ZG? In the datasheet I saw that there are two Op-Amp inside the MCU with gain from 2 to 16. How can I use this Op-Amp? I have to do something about the hardware or I have just to write some code?
2023-10-27 07:36 AM
There are three pins that act as the inputs/output for the op-amp. You have to connect your signals to those pins and use code to configure the OP-Amp as you choose. CubeMX can help with this.
The output is specified as "rail to rail" which in reality typically means a couple mV off from 0-VDDA.
2023-10-27 07:56 AM
Then if I connect the analog output of the micro to the Op-Amp input can I generate a voltage from 0 to 2*Vdda if for example I set the gain of the Op-Amp to 2? Can I do this thing in the interno of micro by software or I have to do an external connection? My need is to generate a controlled analog voltage from 0 to 5 V.
2023-10-27 08:08 AM - edited 2023-10-27 08:09 AM
You can't generate 2*VDDA as the output range is 0-VDDA.
> My need is to generate a controlled analog voltage from 0 to 5 V.
You'll need an external opamp.
2023-10-27 08:51 AM
0-Vdda is the maximum range also for MCU integrated Op-Amp and not only for the analog output?
2023-10-27 09:09 AM
Yes