2024-10-15 03:11 AM
I am writing the code stm32H7ZIT6 based master to control slaves based on LTC6810 ic. Although, I am getting errors while importing the specific LTC libraries needed for making this setup work. I am trying to import specifically these libraries
1. LT6810.h
2. LT681x.h
3. LT_SPI.h
4. Linduino.h
but all these are dependent on arduino-based libraries. I have limited experience with stm32, can you help me with what I am doing wrong.
2024-10-15 03:20 AM
It's not going to be a simple matter of just importing straight into STM32CubeIDE - you're going to have to "unpick" the Arduino/Linduino dependencies.
Note that there is an Arduino core available for STM32:
Might be easier to start by getting this Arduino code into that.
Or just start by getting it working in the standard Arduino IDE on a standard Arduino?
Maybe AD can provide some guidance on that?
2024-10-15 03:29 AM
On adapting Arduino code to STM32CubeIDE (second part of post):
The whole point of the Arduino framework is that it "hides" the underlying hardware details from you, providing platform-independent interface like "wire" for I2C and the SPI library for SPI:
https://docs.arduino.cc/language-reference/en/functions/communication/SPI/
So one way to take Arduino code into other ecosystems (eg, STM32CubeIDE) is to just implement those interfaces...