2024-06-25 7:17 AM
Kudo for Company support. Moving to Nordic Semiconductor!
Solved! Go to Solution.
2024-06-27 12:14 AM
Hi GS2,
this error is detected by the very last GCC (12). this compiler has not been the default for a long time.
BR
2024-07-01 1:30 PM
Thank you Christelle,
With the next release: 1.16.0. - Build Finished. 0 errors, 0 warnings.
2024-07-02 2:57 PM
Have tried to put question on Nordic Semiconductor -- did not get any response, accept automated reply that my question is assigned to employee! But there documentation is much better detailed, also they have both example for BLE_HID - for mouse and keyboard! It is hard to convert this samples to STM32CubeIDE. As I already bought P-NUCLEO-WB55RG - I will try to use it.
2024-07-02 3:19 PM
@GS2 wrote:It is hard to convert this samples to STM32CubeIDE..
Also pointless!
It's an entirely different stack for an entirely different radio. It won't work on an ST chip!
2024-07-03 4:32 AM
It is at times like these is when I miss a down vote button. This topic is a waste of everyone's time.
2024-07-03 3:27 PM
Yes, I would agree with you, if you tell - how to remove this topic!
2024-07-03 3:32 PM
Thank you Andrew again. Now I understand that I need to find other company that have BLE_HID mouse and keyboard examples, or better combo, so I can start developing my wireless controller with an air mouse and custom keyboard!