2025-01-29 2:25 AM - last edited on 2025-01-29 7:29 AM by Andrew Neil
Dear ST Support Team,
I recently purchased the STM32H7S7-DK development board (MB1736D) and I am encountering an issue when attempting to debug my main application code. The error message displayed is:
“Failed to initialize external memory!”
“Error in initializing ST-LINK device.”
I have already configured the external memory loader as per the documentation and have attached pictures for your reference. Despite these configurations, I am unable to proceed with debugging.
Could you kindly assist me in resolving this issue? Furthermore, I would like to know whether it is possible to debug external memory through serial debugging using the onboard ST-LINK, or if it requires another setup.
Additionally, if I plan to use the JTAG interface to debug the development board, could you please inform me of any changes or configurations required to achieve this?
I am looking for solution as soon as possible,
Thank you .
Best regards,
Er. Vijay Kushwah
e.mail : vijaykushwah1112@gmail.com
Company : Gailron Controls Devices,
Faridabad,121003,Haryana,India
2025-01-29 5:25 AM
Hello @VijayKushwah ,
This article will help you on how to debug in external memory on STM32CubeIDE :
Debugging in external memory on STM32CubeIDE - STMicroelectronics Community
For JTAG, check the configuration with the product Datasheet to ensure that the JTAG interface is properly connected to the STM32H7S7-DK board. This involves connecting the JTAG pins (TMS, TCK, TDI, TDO, and TRST) to the corresponding pins on the board. For that, you can check Table 4. JTAG/SWD cable connections on STLINK-V2:
ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32 - User manual