2023-08-13 05:22 AM
[This is a reconstruction of a thread I've started on Mar 26, 2017, but got lost in the two forum software transitions since then.]
Reports in IWDG short period (125 us) problem and STM32F407 : IWDG and erase flash sector indicate that the IWDG does not work as it's (quite simplistically) described in the RM.
To find out the real working of IWDG, I took a DISCO-F4, wrote a snippet which brought out LSI through its connection to TIM5_CH4 onto a pin, wired up a LA and started experimenting.
The following is my interpretation of what I've seen; I don't know what's the real implementation of course so I might have misinterpreted things. I haven't experimented with the debug facility. I haven't used other prescaler than the lowest (i.e. /4) - some of the cycles numbers mentioned below might be dependent on this.
As I've said, this is just a guess how things might work, I don't see the innards of the chip.
ST, please comment.
Thanks,
Jan Waclawek
2023-08-13 09:09 AM
Dear @waclawek.jan ,
Many thanks for the detailed experiments, Once back to office next week , we will feedback with detailed answers and actions .
have a great Sunday !
STOne-32
2023-08-18 02:52 PM - edited 2023-08-18 02:53 PM
Dear @waclawek.jan ,
Greetings and How are you doing today ? After a long and deep investigation with our experts and design teams that took about 5 days including some public holidays. We confirm all of the findings on IWDG and our action plan is on-going to update and communicate via our official documentation :
thank You very much again for your time and patience , if you need early drafts once we approve them internally @Sarra.S can help .
have a great weekend and many many thanks for the valuable contribution .
Ciao
STOne-32
2023-08-18 10:44 PM
Hi @STOne-32 ,
Thanks for letting us know.
> if you need early drafts
Thanks, I don't. I don't use the IWDG, in fact, this was my only "physical" encounter with watchdogs as such so far (although I've written about them in the distant past).
However, what I would very much like to see is an Application Note. I know that means another 5 or more days of work, including FAEs, but I believe it's time and effor well spent. In such AN, I'd like to see a general overview of the topic, including discussion of merits and drawbacks (as they are!) of using WD as such, legislative requirements for its usage; discussion of various forms of WD from hardware single-shots through clocked ones up to complex things like WD-refresh-over-internet; overview of WD implementations in STM32 families; intimate details and relationships such as LSI-autostart-which-does-not; techniques to use IWDG in software and common pitfalls, errors and misconceptions. (Oh, maybe that's not one AN. You may have heard of my "dozens of appnotes per peripheral" mantra...)
JW
2024-03-30 12:53 AM
Hi @STOne-32 ,
I've checked the new RM0090 (rev.20, 07-Feb-2024) and ES0182 (Rev 15, 12-Feb-2024) and I don't see any change in IWDG descriptions there.
JW
2024-03-30 01:05 AM
Hi @waclawek.jan ,
Indeed, as the change is impacting many series the updates relative to IWDG are not yet processed in this RM0090 . Let me check the status and back to you @Sarra.S .
thanks for the patience.
STOne-32