Skip to main content
Associate III
Oct 30, 2024 6:40 AM UTC
Solved

CTSIZE becomes 0x01 after SPI communication is completed

Regarding the problem that CTSIZE becomes 0x01 after SPI communication is completed,

In our program, SPI-SR-CTSIZE becomes 0x01 after SPI communication is completed.
In that state, if we try to perform the next SPI communication, a timeout error occurs in the middle of the communication.
When SPI-SR-CTSIZE = 0, no timeout error occurs.
Is there any way to set SPI-SR-CTSIZE (= TSIZE number of frames in a session) to 0?

Translated with DeepL.com (free version)

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Nov 1, 2024 11:54 AM UTC

Hello @pass3master ,

Did you check if this issue related to SPI errata described in the STM32H7 errata sheet, where setting non-zero TSIZE is observed as Tx traffic, or possible corruption of last-received data depending on CRCSIZE setting.

Note that TSIZE=0 (EOT is never raised) should be used either with single data packet setting or batches always aligned with the packet setting exclusively.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Nov 1, 2024 11:54 AM UTC

Hello @pass3master ,

Did you check if this issue related to SPI errata described in the STM32H7 errata sheet, where setting non-zero TSIZE is observed as Tx traffic, or possible corruption of last-received data depending on CRCSIZE setting.

Note that TSIZE=0 (EOT is never raised) should be used either with single data packet setting or batches always aligned with the packet setting exclusively.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks