cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any free IDE for NUCLEO-H753ZI board?

RongShengWang
Associate III

Hi,

    Is there any free IDE for NUCLEO-H753ZI board?

Thanks,

Peter

 

1 ACCEPTED SOLUTION

Accepted Solutions

There's no need to format your whole post as BOLD!

Yes - as the name suggests, the STM32CubeIDE is for the whole STM32 product range.

View solution in original post

11 REPLIES 11
Pavel A.
Evangelist III

Yes, there is at least one. Can you guess which? ))

Cubemx and Cubemx IDE???

I have been using both for  Nucleo STM32C0.

Andrew Neil
Evangelist III

Thanks Andrew,

There are two choices below - Should I choose the first one - "Patch_CubeH7"???

1. Patch_CubeH7

2. STM32CubeH7

Thanks again!!!

No, there is only one IDE listed there:

AndrewNeil_0-1732008229485.png

As the name suggests, STM32CubeIDE is the IDE.

 


@RongShengWang wrote:

Patch_CubeH7


It's "Pack" - not "Patch".

As it says. it's a software pack with the HAL drivers, etc:

https://www.st.com/en/embedded-software/stm32cubeh7.html

You use that in conjunction with the IDE of your choice.

With CubeIDE, you don't need to download it separately - CubeIDE will download it for you when you start a Project.

Thanks.

I have been using Cubemx and Cubemx IDE for  Nucleo STM32C0. board.

The IDE should be the same for STM32H7, right? Thanks!

 

 

There's no need to format your whole post as BOLD!

Yes - as the name suggests, the STM32CubeIDE is for the whole STM32 product range.

For the STM32C0, and ALL STM32 CM0(+) there's also a free KEIL MDK Licence available.

Doesn't work with CM3/CM4/CM7 cored parts

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

free KEIL MDK Licence doesn't work with CM3/CM4/CM7 cored parts - right?

Thanks,