cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any example code for creating a PDF file in bare-matel

Vijay1
Associate II

I am making temperature data logger using STM32L071, so every week I have to create (non editable) a PDF report from the device. Due to regulation and data protection I can't create this is PC/ Laptop. So only option left is generating pdf report in micro-controller it self.

I tried few option source library i.e https://github.com/AndreRenaud/PDFGen but it requires lot of dynamic memory.

If anyone tried before or knows right way please guide me.

1 REPLY 1
TDK
Guru

Not aware of any bare metal PDF generating code.

"Bare metal" and "PDF" is an atrocious combination. I have to imagine there is a better way to do what you want to do.

If you feel a post has answered your question, please click "Accept as Solution".