2024-07-23 07:55 PM
Hi Community
I am using this STM32H747 and cannot find the project in the "en.stm32cubeh7-v1-11-2". Similar to the use of STM32H743 , I can find the corresponding project in the "en.stm32cubeh7-v1-11-2" . Can you provide the projects
corresponding to STM32H747? thanks !
"en.stm32cubeh7-v1-11-2"
2024-07-23 09:31 PM
Hello @shaunSHAUN and welcome to the ST Community 😊.
Here are the examples for the STM32H747I-EVAL and STM32H747I-DISCO.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-24 01:51 AM
Hello @shaunSHAUN and welcome to the community.
Not clear. These are the folders corresponding to STM32H747 examples.
Could you please explain more the situation?