cancel
Showing results for 
Search instead for 
Did you mean: 

is there a software package about STM32H747 in this STM32H7xxI-Eval

shaunSHAUN
Associate

Hi Community

I am using this STM32H747 and cannot find the project in the "en.stm32cubeh7-v1-11-2". Similar to the use of STM32H743  , I can find the corresponding project  in the "en.stm32cubeh7-v1-11-2"  . Can you provide the projects

corresponding to STM32H747?  thanks !

 

 

"en.stm32cubeh7-v1-11-2"

shaunSHAUN_0-1721789692859.png

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @shaunSHAUN and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Here are the examples for the STM32H747I-EVAL and STM32H747I-DISCO.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

SofLit
ST Employee

Hello @shaunSHAUN and welcome to the community.

Not clear. These are the folders corresponding to STM32H747 examples.

SofLit_0-1721811026964.png

Could you please explain more the situation?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.