2025-03-18 9:21 PM - last edited on 2025-03-21 4:05 AM by Andrew Neil
Hi Everyone,
I interfaced Nucleo F767ZI with W25Q256JV using SPI and everything was working fine. But due to time and speed requirements, now I have to shift it to QSPI. I have used example code of STM Document named "QSPI_F769_discovery_flashloader" and developed a code for QSPI. But whenever I try to run the code and write/read the memory, nothing happens. I started to run code in debug on STMCube IDE and found that when try to send command to enable write and read status register, the register value doesn't change to write enable (0x02).
Always fail here and Error LED turns ON.
if (HAL_QSPI_AutoPolling(&hqspi, &sCommand, &sConfig, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
return QSPI_ERROR;
}
The Write Enable function is here.
uint8_t QSPI_WriteEnable(void) {
QSPI_CommandTypeDef sCommand;
QSPI_AutoPollingTypeDef sConfig;
memset(&sCommand, 0, sizeof(sCommand));
memset(&sConfig, 0, sizeof(sConfig));
/* Enable write operations ------------------------------------------ */
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = WRITE_ENABLE_CMD;
sCommand.AddressMode = QSPI_ADDRESS_NONE;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
return QSPI_ERROR;
}
/* Configure automatic polling mode to wait for write enabling ---- */
sConfig.Match = 0x02;
sConfig.Mask = 0x02;
sConfig.MatchMode = QSPI_MATCH_MODE_AND;
sConfig.StatusBytesSize = 1;
sConfig.Interval = 0x10;
sConfig.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
sCommand.Instruction = READ_STATUS_REG_CMD;
sCommand.DataMode = QSPI_DATA_1_LINE;
if (HAL_QSPI_AutoPolling(&hqspi, &sCommand, &sConfig,
HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
return QSPI_ERROR;
}
return QSPI_OK;
}
Below is my attached qspi.h and qspi.c files and CubeMX configuration.
Kindly help me, what is the problem and if possible provide me a .c .h file for QSPI it's urgent.
Looking forward to suitable response, thanks in advance.
Solved! Go to Solution.
2025-03-18 10:12 PM - edited 2025-03-18 11:23 PM
hii @NajeebUllahKhan
Try following files ... there you may need to change flash size or other some parameters.
To test your quad spi is working or not take reference of following code
void testQSPI(){
QSPI_CommandTypeDef s_command;
uint8_t pData[3];
uint8_t wData[0x100];
uint8_t rData[0x100];
uint32_t i;
printf("***************QuadSPi Example*******************************\r\n");
BSP_QSPI_Init();
/*##-2-Read Device ID Test ###########################################*/
/* Read Manufacture/Device ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_1_LINE;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("SPI I/0 Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Dual I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = DUAL_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_2_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_2_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0;
s_command.DataMode = QSPI_DATA_2_LINES;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Dual I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Quad I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = QUAD_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_4_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_4_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0x00;
s_command.DataMode = QSPI_DATA_4_LINES;
s_command.DummyCycles = 4;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Quad I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read JEDEC ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_JEDEC_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 3;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Read JEDEC ID : 0x%2X 0x%2X 0x%2X\r\n\r\n",pData[0],pData[1],pData[2]);
/*##-3-QSPI Erase/Write/Read Test ###########################################*/
/* fill buffer */
for(i =0;i<0x100;i ++)
{
wData[i] = i;
rData[i] = 0;
}
if(BSP_QSPI_Erase_Block(0) == QSPI_OK)
printf(" QSPI Erase Block ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Write(wData,0x00,0x100)== QSPI_OK)
printf(" QSPI Write ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Read(rData,0x00,0x100)== QSPI_OK)
printf(" QSPI Read ok\r\n\r\n");
else
Error_Handler();
printf("QSPI Read Data : \r\n");
for(i =0;i<0x100;i++)
printf("0x%02X ",rData[i]);
printf("\r\n\r\n");
for(i =0;i<0x100;i++)
if(rData[i] != wData[i])printf("0x%02X 0x%02X ",wData[i],rData[i]);
printf("\r\n\r\n");
/* check date */
if(memcmp(wData,rData,0x100) == 0 )
printf(" W25Q128FV QuadSPI Test OK\r\n");
else
printf(" W25Q128FV QuadSPI Test False\r\n");
}
2025-03-18 10:12 PM - edited 2025-03-18 11:23 PM
hii @NajeebUllahKhan
Try following files ... there you may need to change flash size or other some parameters.
To test your quad spi is working or not take reference of following code
void testQSPI(){
QSPI_CommandTypeDef s_command;
uint8_t pData[3];
uint8_t wData[0x100];
uint8_t rData[0x100];
uint32_t i;
printf("***************QuadSPi Example*******************************\r\n");
BSP_QSPI_Init();
/*##-2-Read Device ID Test ###########################################*/
/* Read Manufacture/Device ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_1_LINE;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("SPI I/0 Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Dual I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = DUAL_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_2_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_2_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0;
s_command.DataMode = QSPI_DATA_2_LINES;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Dual I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Quad I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = QUAD_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_4_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_4_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0x00;
s_command.DataMode = QSPI_DATA_4_LINES;
s_command.DummyCycles = 4;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Quad I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read JEDEC ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_JEDEC_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 3;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Read JEDEC ID : 0x%2X 0x%2X 0x%2X\r\n\r\n",pData[0],pData[1],pData[2]);
/*##-3-QSPI Erase/Write/Read Test ###########################################*/
/* fill buffer */
for(i =0;i<0x100;i ++)
{
wData[i] = i;
rData[i] = 0;
}
if(BSP_QSPI_Erase_Block(0) == QSPI_OK)
printf(" QSPI Erase Block ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Write(wData,0x00,0x100)== QSPI_OK)
printf(" QSPI Write ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Read(rData,0x00,0x100)== QSPI_OK)
printf(" QSPI Read ok\r\n\r\n");
else
Error_Handler();
printf("QSPI Read Data : \r\n");
for(i =0;i<0x100;i++)
printf("0x%02X ",rData[i]);
printf("\r\n\r\n");
for(i =0;i<0x100;i++)
if(rData[i] != wData[i])printf("0x%02X 0x%02X ",wData[i],rData[i]);
printf("\r\n\r\n");
/* check date */
if(memcmp(wData,rData,0x100) == 0 )
printf(" W25Q128FV QuadSPI Test OK\r\n");
else
printf(" W25Q128FV QuadSPI Test False\r\n");
}
2025-03-19 1:41 AM
OK, let me check and I'll update my code accordingly and then will let you know.
Is the code you provided has tested before?
2025-03-19 2:18 AM - last edited on 2025-03-19 2:22 AM by mƎALLEm
I have tested it and made some changes but still not working. When I used the "void testQSPI()" function to check if QSPI is working, it is not working as "static uint8_t QSPI_AutoPollingMemReady(uint32_t Timeout)" this function give QSPI_ERROR on the line
if (HAL_QSPI_AutoPolling(&QSPIHandle, &s_command, &s_config, Timeout) != HAL_OK)
{
return QSPI_ERROR;
}
in QSPI_AutoPollingMemReady(uint32_t Timeout).
below is my attached updated files. and debug results.
Looking forward to your response...
2025-03-19 2:21 AM
Hello @NajeebUllahKhan,
Please use </> button to share your code.
See this post.
Thank you for your understanding.
2025-03-19 11:20 PM
@NajeebUllahKhan wrote:Is the code you provided has tested before?
Yes it is tested. make shure you have configured QUAD SPI properly in the cubeMX. it should be like this:
Quad SPI W25Qxx Config
2025-03-20 11:21 AM
I am getting 0 0 0 on reading ID and when compare wdata, rdata, it goes into else and rdata shows 0 0 0 ..., below is all details. Now one thing is confirmed that the code runs fully without any error but now problem is, chip is not giving any information like ID etc which always is 0 0 0 etc. I am using W25Q256JV 32MB with Nucleo F767ZI with HSI CLK Source and with 216 MHz. Find all details below.
I am using following PINS:
CS -> PB10, CLK -> PB2, I0 -> PD11, I1 -> PD12, I2 (WP) -> PE2, I3 (HLD) -> PD13, rest I am using your files without any change and your test function.
Kindly assist me in this, it's very urgent for me.
2025-03-20 6:57 PM
QSPI_CommandTypeDef s_command = {0}; // clear the auto/local variable in all instances
2025-03-20 10:29 PM - edited 2025-03-20 11:34 PM
This code i use to test Custom boards that having quadspi... in some boards, if QuadSPI Test gets faild i suspect there is hardware issue present in the boards .. so i hand over those boards to hardware team.. But in my case all software configurations are correct. as your telling that with SPI its working then you need to confirm your config parameters.
I have sucessfully tested F746 and H743 boards with this code. BTW we are using W25Q128 that is 16MB flash thats why i taken Flash size in CubeMX as 23.
2025-03-22 12:02 AM
@jumman_JHINGA @Tesla DeLorean
I am following this link "https://os.mbed.com/platforms/ST-Nucleo-F767ZI/" to check out connection on my F767ZI board. As there is only QUADSPI in this board which can be mapped on the pins highlighted in the link.
I am using following PINS:
CS -> PB10, CLK -> PB2, I0 -> PD11, I1 -> PD12, I2 (WP) -> PE2, I3 (HLD) -> PD13, comparing this with pins mentioned in the link, do you see any connection problem on F767ZI board side? If not, then maybe it's on the flash side. Highlighted pins in the picture are used.
QSPI configurations are below.
Sys Clk configurations are below.
These are all my configurations. Rest I am using all yours code without any change.
1) Does Sys Clk configuration have any error?
2) Does there is any connection issue on Board side like wrong pin for QSPI?
3) Does QSPI software configuration have any error?
4) If I use same code for 32MB flash, will it work (because commands are same throughout winbond W25Q series right?)? If yes, then upto 16MB region.
Looking forward to your assistance...