cancel
Showing results for 
Search instead for 
Did you mean: 

Error on Reference Manual for STM32F411xx for RCC Register Map Table

anardinelli
Associate II

Hi all,

I'd just like to report an error on the reference manual for RMSTM32F411 (RM 0383 Rev 3).

The error is located on page 471, on section RTC Register Map.

The table showcase all registers for the RCC and miss the entry for RTC_SHIFTR (located at address offset 0x2C) and also for RTC_TSDR (located at address offset 0x34).

Screenshot from 2025-04-07 18-20-31.pngScreenshot from 2025-04-07 18-22-21.png

 

Here, 0x2C and 0x34 are missing from the register map.

 

Screenshot from 2025-04-07 18-21-47.png

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @anardinelli and welcome to the community;

 

Thank you for bringing this issue to our attention.

I reported internally.

Internal ticket number: 207011 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hello @anardinelli and welcome to the community;

 

Thank you for bringing this issue to our attention.

I reported internally.

Internal ticket number: 207011 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.