2024-07-04 03:06 AM - edited 2024-07-04 03:07 AM
Hello,
I am using the sbsfu application. Once I have implemented the SBSFU firmware to the board, when I connect the board to the STM32Cubeprogrammer, the SBSFU application is in lock status because it has detected an intrusion. I would like to add a printf warning about the intrusion as soon as possible when this situation happens or when someone unauthorized tries to update the firmware. Is it possible to do the following and where should I add it?