cancel
Showing results for 
Search instead for 
Did you mean: 

in 'H7 RMs, incorrect ITR description for OTG USB SOF-to-TIMER, in figure caption

(Spotted by sx107.)

I know the subject is not very descriptive, but a figure is worth 1000 words:

waclawekjan_0-1723554179710.png

It's also in other 'H7 RMs; I leave it to ST to check them all :)

(Btw. this is a carryover from the 'F7 RM, where both OTG's SOF indeed feed into TIM2 ITR1, through a mux controlled by a bitfield in TIM2_OR.)

JW

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @waclawek.jan 

Thank you for reporting this inconsistency.

An internal ticket 188629 is submitted to review and update RMs including RM0399 RM0433 and RM410... 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @waclawek.jan 

Thank you for reporting this inconsistency.

An internal ticket 188629 is submitted to review and update RMs including RM0399 RM0433 and RM410... 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.