2024-08-13 06:04 AM - edited 2024-08-13 06:05 AM
(Spotted by sx107.)
I know the subject is not very descriptive, but a figure is worth 1000 words:
It's also in other 'H7 RMs; I leave it to ST to check them all :)
(Btw. this is a carryover from the 'F7 RM, where both OTG's SOF indeed feed into TIM2 ITR1, through a mux controlled by a bitfield in TIM2_OR.)
JW
Solved! Go to Solution.
2024-08-13 06:49 AM
Thank you for reporting this inconsistency.
An internal ticket 188629 is submitted to review and update RMs including RM0399 RM0433 and RM410...
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-13 06:49 AM
Thank you for reporting this inconsistency.
An internal ticket 188629 is submitted to review and update RMs including RM0399 RM0433 and RM410...
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.