2019-11-29 6:50 PM
2019-12-16 10:56 AM
The connector and silk-screen suggest it is a 20-pin JTAG header, would connect to an ST-LINK/V2 or J-LINK type pod.
2019-12-16 2:03 PM
sorry, but what is ST-LINK/V2 or j-LINK
2019-12-18 2:05 PM
How to find out if it is ST-LINK or J-LINK?
2019-12-18 2:14 PM
Either, should I Google this stuff for you?
It is a header you'd plug the aforementioned debug pods into.
Perhaps you could refer to the schematic for your board, of docs from its manufacturer.
2019-12-18 2:23 PM
Thanks. The Eng'r working on this quit just gave me the board with no schematics just block diagrams. So, I don't know which terminals of the MCU are used for programming the MCU. Any help appreciated.
2019-12-18 2:32 PM
2019-12-18 2:50 PM
I DO HAVE THE JTAG pin #s if that helps
2019-12-19 3:12 PM
Can the functions of JTAG be programmed in the MPU? Or does JTAG have to be a separate HW device?
2019-12-19 3:47 PM
Usually it is a separate device. Is Google blocked in your school or workplace?
-- pa
2019-12-19 4:50 PM
Thanks. Thought this was a helpful site. Yes I did google but no clear cut answer. I can show you my schematic where the JTAG is implemented in the MCU, hence I was not sure