cancel
Showing results for 
Search instead for 
Did you mean: 

I want to use the STM32G474VET6 in a robotic application with 3 motors and a diff GPS. Can I program it in Assembly or do I use C? If the latter is Keil a good compiler?

KDIAS.2340
Associate II
 
49 REPLIES 49

The connector and silk-screen suggest it is a 20-pin JTAG header, would connect to an ST-LINK/V2 or J-LINK type pod.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KDIAS.2340
Associate II

sorry, but what is ST-LINK/V2 or j-LINK

KDIAS.2340
Associate II

How to find out if it is ST-LINK or J-LINK?

Either, should I Google this stuff for you?

It is a header you'd plug the aforementioned debug pods into.

Perhaps you could refer to the schematic for your board, of docs from its manufacturer.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KDIAS.2340
Associate II

Thanks. The Eng'r working on this quit just gave me the board with no schematics just block diagrams. So, I don't know which terminals of the MCU are used for programming the MCU. Any help appreciated.

tHANKS
KDIAS.2340
Associate II

I DO HAVE THE JTAG pin #s if that helps

KDIAS.2340
Associate II

Can the functions of JTAG be programmed in the MPU? Or does JTAG have to be a separate HW device?

Usually it is a separate device. Is Google blocked in your school or workplace?

-- pa

KDIAS.2340
Associate II

Thanks. Thought this was a helpful site. Yes I did google but no clear cut answer. I can show you my schematic where the JTAG is implemented in the MCU, hence I was not sure