cancel
Showing results for 
Search instead for 
Did you mean: 

I have STM32F031F4P7 microcontroller with USART1_Tx defined on two pins PA9 and PA14. So can we use USART1_Tx of both pins at the same time?

AKadi.1
Associate II
 
2 REPLIES 2
Danish1
Lead III

Try it.

You probably can’t do it through HAL calls because it’s such an unlikely desire.

I suggest you look in the References Manual for how to select Alternate Functions for the GPIO pins. And the Data Sheet for which AltFunction number you need for USART1.

I don’t know if it will work. It depends on the detail of how ST chose to implement the AltFunction circuits, and might differ between stm32 families. (A reason it might not work is if ST chose to prevent inputs from being abused in the same way).

Hope this helps,

Danish

My take on this.

JW​