2023-11-19 09:11 PM
Hi
In the figure below, FIFO1 filter bank 7 and filter bank 10 have the same settings. If the ID list is 16bit, I think it is correct to have 4 Filter Nums. There are two filter banks 7, 4 and 5. Is this correct?
Solved! Go to Solution.
2023-11-22 06:30 AM
Hello @Ukazu ,
Thank you fringing this issue to our attention.
Figure 394. in RM0316 is wrong and should be:
Filter bank 7 and filter bank 10 haven't the same settings.
Filter bank 7: Deactivated ID Mask (16-bit), Filter Num 4, 5
Filter bank 10: Deactivated ID List (16-bit), Filter Num 8,9,10,11.
I reported this typo internally.
Internal ticket number: 166948 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-20 08:22 AM
Hi @Ukazu ,
Thank you for posting this issue.
I will check internally and I will get back to you with more details as soon as possible.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-22 06:30 AM
Hello @Ukazu ,
Thank you fringing this issue to our attention.
Figure 394. in RM0316 is wrong and should be:
Filter bank 7 and filter bank 10 haven't the same settings.
Filter bank 7: Deactivated ID Mask (16-bit), Filter Num 4, 5
Filter bank 10: Deactivated ID List (16-bit), Filter Num 8,9,10,11.
I reported this typo internally.
Internal ticket number: 166948 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-26 03:45 PM
Thank you.
This modification is as per the documentation.
I have no doubts.
This thread will be closed.