2020-06-08 9:21 AM
Hello guys.
As indicated in the title, I have an STM32H7B3I-DK board here with me. I am trying to play with it but currently having a hard time to load the code to the board from Keil MDK v5.23. When I compile the project and press a Download button, I get Internal Command error as indicated bellow:
ST-Link Debugger is selected for Debugger in Keil uVision project:
Also, I used ST-Link Upgrade to upgrade ST-Link firmware to the latest version. The board seems to be functional because I can connect to it and program it using STM32CubeProgrammer but not with Keil MDK.
Do you have any idea what I might be doing wrong?
I used Keil MDK with Nucleo-F401RE board without any problem.
Thanks in advance for your time and efforts.
Sincerely,
Bojan.
Solved! Go to Solution.
2020-06-08 9:34 AM
>>Keil MDK v5.23
VERY OLD
Get 5.29, use the ST-LINK drivers, DLLs and support from that. This board uses an ST-LINK V3, you need software that is sufficiently aware of this.
\KEIL\ARM\STLINK
STLinkUSBDriver.DLL
ST-LINKIII-KEIL_SWO.DLL
2020-06-08 9:34 AM
>>Keil MDK v5.23
VERY OLD
Get 5.29, use the ST-LINK drivers, DLLs and support from that. This board uses an ST-LINK V3, you need software that is sufficiently aware of this.
\KEIL\ARM\STLINK
STLinkUSBDriver.DLL
ST-LINKIII-KEIL_SWO.DLL
2020-06-08 11:35 AM
Hey, @Community member !
Thanks for your reply. With Keil v5.30 it is working like a charm! :)
Cheers,
Bojan!