2022-05-30 10:17 PM
2022-06-03 06:21 AM
Hi @Community member ,
I suggest you follow the steps described in Custom Signal generation using PWM and DMA. This can answer your need.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-03 07:52 AM
Check what DMAMUX type sources are described in the Reference Manual, then use those...
2022-06-03 01:53 PM
You can't, at least not directly and not in 'H743 and kin. The MDMA triggers are fixed:
The indirect way would be to trigger any dummy single-transfer with the timer in DMA1/DMA2, and then the transfer complete would trigger MDMA.
JW