Skip to main content
SR NA.2
Associate II
June 2, 2022
Question

Product longevity of STM32F76xx

  • June 2, 2022
  • 5 replies
  • 1840 views

Kindly provide Product longevity of STM32F76xx series MCU

This topic has been closed for replies.

5 replies

Peter BENSCH
ST Technical Moderator
June 2, 2022

Welcome, @SR NA.2​ , to the community!

for all STM32, including the STM32F76xx, there has so far been a rolling commitment for guaranteed production over the next 10 years, currently guaranteed until at least 2032.

However, one must not confuse longevity with scarce current availability.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
June 3, 2022

Perhaps convey to management that ST needs to start getting a lot more transparent in what it's plans are moving forward here.

With 12, 18 or 24 months of runway at lot of us are likely to decamp and find alternatives in the mean-time, and ST's going to be out of the design refresh.

Most companies dealing with consumer products don't work on 10 year availability expectations, or don't have staff retention to sustain that. All the institutional knowledge leaves or gets fired.

Vendors like Micron have a limited subset of parts they guarantee availability on, and one of their strategies is to die-shrink to reduce cost, and expand availability, via equivalent form and function.

Is there some prospect that the F1 or L1 families will be die shrunk onto tighter geometries?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Technical Moderator
June 3, 2022

@Community member​ 

Very interesting question!

Several points have to be taken into account:

  • While memory devices are high-density logic, they are much less complex in terms of different functions than general-purpose microcontrollers, and they are not mixed-signal designs. If you were to shrink a microcontroller, this would also result in different parameters of the analogue functions, which would then no longer be in accordance with the original data sheet, resulting in a completely new component that would have to be completely re-qualified.
  • In addition, the STM32F1 and STM32L1 are based on the Cortex-M3, which is no longer used by ST in new MCUs.
  • Another point: the so-called pad limitation. If you make the core logic smaller, at some point the area required for the pads of the bond wires outweighs the space, which makes the process no longer economically viable.

So does it really make sense to think about smaller structures in MCUs?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
June 3, 2022

Clive,

note, that some of it is just glitter, not gold. The 45nm node comes with drawbacks. Good for gadgets, bad for the slightly better stuff.

JW