cancel
Showing results for 
Search instead for 
Did you mean: 

HRTIM v2 - PWM higher than 16 bits

Mac
Associate

I'm using HRTIM to generate 16 bit duty cycle PWM on a G474, it works nicely.

How can I configure the HRTIM to do more than 16 bit duty cycle?

I've read the HRTIM cookbook and had a look at what configuration options are available in the HAL. I was hoping to find something like the ability to use the crossbar to apply a SET upon the result of a logical AND of two input signals (coming from 2 compare registers) but no luck.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mac
Associate

Update: I was able to use the Burst DMA feature to achieve this.

Singh.Harjit
Senior II

Can you elaborate, please?