cancel
Showing results for 
Search instead for 
Did you mean: 

Bug report - HRTIM ADC Trigger post scaler STM32G474

PDvor.2
Associate

Hello

HRTIM´s ADC Triggers post scalers on STM32G474 have 5 bits (0..31) , but in CubeMX you can set 10 bits (0..1048575). Upper bits are trimed so it can be confusing when you set value above 31.

 

My versions:

STM32CubeMX Version: 6.15.0-RC7 Build: 20250701-1659 (UTC)

STM32Cube MCU Package for STM32G4 Series  1.6.1

STM32CubeIDE Version: 1.19.0

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @PDvor.2 

 

First let me thank you for posting.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @PDvor.2 ,

 

Let me thank you for bringing this issue to our attention.

An internal ticket is submitted to the development team ( Internal Ticket Number: 220814 ).

I will let you know when this issue is solved.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.