2024-07-03 01:08 AM
Hi All,
I use VSCode+STM32 plug-in and it works great, however, one problem I have is that every time I run STMCube32mx it updates the cmake file (CMakeLists.txt). There is no /*USER CODE */ section in this file so I have to constantly fix the CMakeLists.txt file with my additions.
I checked STM32CubeMX project manager settings and there is no option to not generate a build file and there are no options to add your settings.
Any idea?
Thanks,
Hans.