cancel
Showing results for 
Search instead for 
Did you mean: 

how to configure the adc internal reference voltage??

Vel
Associate III

Hi team,

I am using STM32L052K8U6 package in my design. I need to configure the internal reference voltage instead of external reference voltage for ADC. Can i get any example program for same.

2 REPLIES 2
Uwe Bonnes
Principal III

VREF for the ADC is always VREF or VDD(A) if there is no VREF pin. However you can measure VREF internal with the ADC and the scale the other measured voltages.

Hi,

In my 32 pin device don't have VREF pin and I need to use my internal reference voltage 1.22V as my ADC reference.