cancel
Showing results for 
Search instead for 
Did you mean: 

How can I change the "Maximum output speed" for the GPIO output to toggle faster ?

YSall.1
Senior

I tried to get the minium delay between output state but I am limited by the GPIO toggling speed, I even tried PWM generation and there is an option on GPIO settings -> Maximum output speed but I can't change it by clicking on it.

Does anybody has an idea on how to set up the maximum speed for GPIO Output?

7 REPLIES 7
Peter BENSCH
ST Employee

This is essentially the same question you asked here. It's probably clearer to finish discussing the topic there and stay in one thread.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
YSall.1
Senior

Okay no problem

It's just that my question here is more precise

@Peter BENSCH​ 

It's probably clearer to finish discussing the topic there and stay in one thread.

All very well, Peter. But someone has marked that question as answered so those who feel able to help might not look at it to see there's a supplementary question

> there is an option on GPIO settings -> Maximum output speed but I can't change it by clicking on it

This to me sounds like question on CubeMX and its quirks and limitations.

JW

Thank you for having replied to my question in the other topic

You're right