2024-07-25 09:59 AM - edited 2024-07-26 03:12 AM
Hi i plan new design and require activate for example on PA3 ADC1_IN4 and same time COMP2_INP.
Is this possible and if yes how sequence to setup HAL LL or direct?
EDIT: Renamed from more AF ... only one AF poss.
2024-07-26 02:57 AM
No. Cube is right. (here
See rm : setting the AF ...ONE value per pin - so its ONE AF possible . dot .
2024-07-26 03:03 AM
I agree one AF, but disagree many Analog. As is showed on your screens analog is always connected, next in MX you can see + GPIO_Analog not selected and this result i can set AF input capture TIM and manualy set ADC and COMP.
2024-07-26 03:11 AM
No.
see basic pin decision:
IF set to analog...you see yourself.
2024-07-26 03:14 AM
No i set primary AF 10 mode
2024-07-26 03:21 AM