2022-10-20 5:11 AM
I would be happy for recommendations.
kind regards
Benjamin
Solved! Go to Solution.
2022-11-08 7:24 AM
Hello @Benjamin Brammer,
I recommend you the MCU Finder to select the suitable STM32.
I hope this helps!
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-11-08 7:24 AM
Hello @Benjamin Brammer,
I recommend you the MCU Finder to select the suitable STM32.
I hope this helps!
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-11-08 8:03 AM
In addition to what Kaouthar said: the requirements apply to both requested families and the choice depends on other requirements, e.g. any automotive qualification required.
The STM32s do not have AEC qualification, but they support everything else, including SAFERTOS (via partner Wittenstein) and SIL (via X-CUBE-STL).
Regards
/Peter
2022-11-08 10:11 AM
> MEMS compatible
That is a non-sense requirement. MEMS is a general technology, not a specific device type, protocol, standard etc.
2022-11-08 11:13 AM
Thanks, I will have a look at it.
2022-11-08 11:17 AM
thanks for the clarification. I was not sure if MEMS technology uses certain communication interfaces. But I think, it's mostly some serial connection like I²C or SPI.
2022-11-08 11:17 AM
Thanks for the clarification. Well, at the current project state it is not lcear what SIL have to be fulfilled. AEC is not a must, but since AEC components can also qualify for SIL, I thought the SPC5 series might be a look worth, but I thought they were qualified.