2020-07-28 09:31 AM
2020-07-30 12:53 PM
@Community member , Here I am going to use the wire.h library written for i2c connection. Also the pins used for SDA and SCK are as follows:
Is it true to use these two pins for i2c?
The problem I am getting is "error compiling"
Thanks
2020-07-30 01:11 PM
You might want to edit that when you get home, guessing you're on a phone, or having a stroke, or drunk
2020-07-30 01:17 PM
D1 PA9 I2C1_SCL
D0 PA10 I2C1_SDA
Yes..
"Error Compiling" going to need to be more specific about the lines and code the compiler is complaining about.
Can't help you with Arduino, using Keil and C here.
2020-07-30 02:54 PM
Moved here now https://community.st.com/s/question/0D53W00000EDDzhSAH