2021-06-26 10:56 AM
Hello! Just a quick question, I just need some help figuring out what is what.
I am coming from the I2S peripheral and setting up the SAI peripheral and to use the I2S protocol, it's that not straight forward.
I am curious if anyone can tell me what is what
The SAI has
Audio Data Size
Frame length
and Slot numbers
For the I2S equivalents I believe
Audio Data Size = DATALEN
Frame Length = CHANNEL LENGTH
But what the heck is slots?
2021-07-01 8:39 AM
Hello,
Could you please which product you are using please ?
You can refer to the following peripheral presentation as introduction:
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-07-03 6:29 AM
Slots are channels. Everything else is very clearly illustrated in a RM figure mentioned in my previous answer...