Hello Michal,What you are observing may be relative to the Miller effect inside the comparator circuitry.Would it be possible for you to set bit#1 (not documented) in COMP_CxCSR, it enables a compare feature which hold the comparator output during th...
Hello,This is relative to nodeRed version changes. It looks it is need now to add "var" declaration with new variable to avoid error. It looks there is no parameter in STM32CubeMonitor to avoid this code update.I will update the example on my side. R...
Hello,You can refer to ES0499 - Rev 8 which is the errata sheet document of STM32U575x for ADC limitationsI confirm the STM32U575X is not concerned by the mentioned STM32L4 ADC limitation.Regards,Simon
Hello,To answer your question #1 and #2, there is no specified information in the errata sheet because the dummy conversion can be done on any channel with any sampling time configuration : just any dummy conversion is sufficient to recover the issue...