2025-03-17 9:39 AM
We have a device which connects to two other devices as a central, and also is connected to by a third device (Mobile Phone) as a peripheral.
When updating the Bluetooth firmware binary from version 1.20.0 to 1.21.0 we have started experiencing disconnections from the third device, downgrading back to 1.20.0 resolves any issues.
A summary of the connection flow is detailed below:
This behaviour is not observed, and the connection seems to be stable when Device C only connects to one of Device A or B before connecting to Device D, it also seems stable if the following sequence is performed:
This suggests to me that it relates to the order in which devices are connected, however there could be other factors.
Has anyone else experienced anything similar, or got any suggestions on test I could perform to narrow down the cause.
Many Thanks, Graham
2025-04-09 10:22 AM
Hello @Graham1
Could you please give as more details (what you have received as logs, what are FWs that you are using, ...).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.