2014-04-02 3:05 AM
hello everyone
i have adc ad1877, configured as in picture2014-04-04 6:48 AM
Perhaps you have just locked out yourself.
Check the relevant supply voltages on the board, and if o.k., try a mass erase with the Flash Loader Demonstrator, after booting it into system bootloader. There are several threads about this procedure here ...2014-04-05 2:29 AM
Whatever...
In adc datasheet says that reset pulse should be made synchronous to clkin (mcko) . How to make it? By using some interrupt or what?2014-04-05 8:32 AM
In adc datasheet says that reset pulse should be made synchronous to clkin (mcko)
Not really. It says you should do this if you have more than one ADCs and want them all to leave the reset state at the same time. However, I still can't understand the fuzz about a 28-pin, 5V device. Perhaps the signal levels (3.3V <--> 5V) are part of your problems ...
2014-04-05 11:30 PM
Maybe, next time i'll try ad1871, it has independent power supply for i/o which can be powered from 3 volts
2014-04-06 6:19 AM
Seriously, I would consider this 3.3V/5V difference as possible source of your problems.
While the STM32 pins might be 5V tolerant and even read signals correctly, the output signals to the ADC might not reach the L/H theshold. That is a perfect recipe for spurious trouble misbehavior of the ext. device, and lots of new grey hairs. Consider level shifting circuitry, or rather another ADC.