cancel
Showing results for 
Search instead for 
Did you mean: 

Help to do a adc/dma project in stm32f469 disco kit in stm32CubeIde 1.10.1

neuberfran
Associate III

https://www.youtube.com/watch?v=LZIcvYmgGZ8&t=228s

I need to make this video project (which uses stm32f407VGT6) in my stm32f469 disco kit in stm32cube ide 1.10.1

I need step by step

Look below for the stm32f469 mcu typing splash screen. There are several options. The chip I normally work on is this: STM32F469NI...

In the quoted video, the author works with pa1 on stm32f407vgt6. What would be the equivalent on the stm32f469 disk kit?:

19 REPLIES 19

Hi @neuberfran​,

You can use STM32CubeProgrammer tool.

0693W00000VOFFcQAP.jpg 

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
neuberfran
Associate III

@Imen DAHMEN​ 

You still haven't answered the main question I asked above: Why when I move the potentiometer Isn't it changing anything in the value of the dma-adc variable in debug? (Because in the video it works ok.)

@Imen DAHMEN​ 

This image is really bad, I can't even see it with zoom

neuberfran
Associate III

@Imen DAHMEN​ 

You still haven't answered the main question I asked above: Why when I move the potentiometer Isn't it changing anything in the value of the dma-adc variable in debug? (Because in the video it works ok.)

neuberfran
Associate III

@Imen DAHMEN​  Can you help-me more or not?

???

?

Did you even look at the schematic for your board? A1 is an Arduino pinout. Your pot is connected to PORTC pin 2.

If you want to connect the pot to PA1, then you need to use pin D3 on the Arduino connector.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

@Community member​ still didn't work. I also tried to move the Gnd input to the Arduino pins side. nothing solved

@Community member​ still didn't work. Please post 1 video with any stm32f4xx disk kit and potentiometer. And also debug adct this variable result. Something like the video below that is the reason for this issue:

https://www.youtube.com/watch?v=LZIcvYmgGZ8&t=228s

@Community member​ 

I solved with D3 and also when I created the project correctly

0693W00000WHvivQAD.png

Good to hear you got it working :grinning_face:

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.