Help in writing a bare metal code for implementing a UART RX interrupt routine in SMT32F767ZI ?
I started writing embedded code 7 months back for a robotics project. Till now , I was able to handle most of the stuff with HAL libraries. I hit a snag when trying to interface with a AHRS(Microstrain CX5-25) unit. There were time when only first few bytes will be received and the device won't receive any more bytes, even thought the IMU status shows streaming. Suspecting something is wrong with the IMU, I tried reading it from PC using Pyserial and it worked. I suspect something is wrong with HAL Receive IT Function call.
Either way,After inputs from previous posts regarding handling of frames with different sizes. I decided to shift to bare metal register based programming at least for interfacing this device.
Currently I have the following hardware setup.
STM324767ZI Nucleo Uart 5 port is connected to pc via USB-TTL device. I will be using pyserial from PC side to send some arbitrary data. This will help me check the Uart receive isr routine written in STM32 micro controller.
Initial peripheral initialisation code is set using cubemx pre-generated code.
In main.c
I call
__HAL_UART_ENABLE_IT(&huart5,UART_IT_RXNE);
__HAL_UART_ENABLE_IT(&huart5,UART_IT_ERR);
to enable interrupts
Then I write a customisr routine which is called from
void UART5_IRQHandler(void)
custom_isr(UART_HandleTypeDef * huart)
{
uint32_t isrflags = huart->Instance->ISR;
uint32_t crlits = huart->Instance->CR1;
if (((isrflags & USART_ISR_RXNE) != RESET) )//&& ((crlits & USART_CR1_RXNEIE) != RESET))
{unsigned char a = huart->Instance->RDR;
store_ring (a , rbuf);
}
}
I could verify that when ever, I send a byte from pc. The interrupt is triggered, But RDR register is empty.
When I checked the ISR register following bits were set : IDLE,TC complete,Transmit Data,End of Block,Busy flag,character match flag.
Strangely I have enabled interrupt only for error and rx not empty. However after interrupt trigger, when I check the ISR flag, rx not empty flag is not set.
I think, I am making a mistake in the sequence of how its done. Can any one advice on what I am missing ?
Thank you
Yours Sincerely,
S.Shyam