2023-10-06 06:02 AM
Hello,
I was just shocked to see that H723 and H735 are NOT pin-to-pin compatible, at least in LQFP-144.
Shoot, I thought I could switch between H723 / 725 / 733 / 735 if necessary.
I found the list for F4 / F7 / H7 compatibility, is there another list for compatibility within the H7 families?
Solved! Go to Solution.
2023-10-06 06:15 AM
CubeMX will list pin-compatible parts. Load your chip, configure it if you want, then go to Pinout -> List Pinout Compatible MCUs.
2023-10-06 06:15 AM
CubeMX will list pin-compatible parts. Load your chip, configure it if you want, then go to Pinout -> List Pinout Compatible MCUs.
2023-10-06 06:15 AM
Okay, I just found that package compatibility is between H723 and H733, and again between H725 and H735.
What about H7A / B ?
Anyway, an official list would help.
2023-10-06 06:17 AM
@TDK thanks for the hint, but for a quick check that takes too long - at least my CubeMX always needs some time.
I like pdf! :D
2023-10-06 06:18 AM
Hello @LCE
You can use CubeMX Pinout compatible feature to find the list of pin-to-pin compatible MCUs.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-09 04:14 AM
So there's no pdf / app-note about compatibility?
2023-10-10 12:46 AM
Hello @LCE
I would suggest checking out AN5293. It may be helpful 😉
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-10 03:15 AM - edited 2023-10-10 07:53 AM
Thanks, I got that one, and there were comparisons from F7 to H7, but no direct H7-type comparisons.
Now I know what I need, H723 / H733 are compatible, but not to H725 / H735, which I will probably choose because of the BGA packages and the Crypto hardware (H735), just in case I might need it in the future.