cancel
Showing results for 
Search instead for 
Did you mean: 

'H7 ADC offset correction in oversampling mode

Which one is true?

0690X00000AqP9lQAF.png

JW

2 REPLIES 2
Byann.1
Associate II

I'm facing to the same problem. I tried to use hardware oversampling and offset but I could not get the good conversion. 

As show in the previous post with some screenshot of the reference manual,  I don't know if it's possible or not.

Please find also below, another sentence describing some restrictions on oversampling.

Byann1_0-1706022625299.png

Finally my question: is it possible to use both oversampling and offset?

If yes, how to use it and what are exactly the restrictions?

Thanks in advanced for your help

 

 

Imen.D
ST Employee

Hello @Byann.1 ,

Please refer to the last release of RM0433 which contains update and correction.

The contradiction in the RM0433 Rev6 mentioned by waclawek.jan was already corrected in the Section: "Single ADC operating modes support when oversampling" to remove the mention that the offset correction is not supported in oversampling mode.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen